inverter output voltage problem

hello,

I am using the official program "Vector Control of Three-Phase Induction Motor Used in Driving a Pump RX66T Implementation Rev.1.10 - Sample Code". I want to adjust the output voltage of the inverter to 220V. However, if I want to adjust the output voltage to 180V, which part of the program should I modify? I think it is the modulation factor mentioned in this file  page 13, but I can't find the relevant place in the program. How can I achieve 180V?

file:

https://www.renesas.cn/cn/zh/document/apn/vector-control-three-phase-induction-motor-used-driving-pump-rx66t-implementation-rev110

Best Regard,

eva

Parents Reply Children
No Data