Random Address Read eeprom M24256

Hi,

I am trying to read and write eeprom M24256.

I have used smart configuration but I am not able to read data in random address read.

Datasheet related eeprom said:

Random Address Read:

A dummy write is performed to load the address into the address counter. Then, without sending STOP condition, the master sends another START condition, and repeats the Device Select Code, with the RW bit set to 1. The memory acknowledges this, and outputs hte contents of the adressed byte. The master must not acknowledge the byte output, and terminates the transfer with stop condition.

Could you indicate to me how can manage this situation ?

Br,

Parents
  • To address that kind of communication you need to write customized code based on registers. unfortunately, the prewritten functions and smart configuration setup don't allow for that kind of sequence, as it automatically sends stop and start conditions. and you might get into trouble if modify the smart code generator codes.

    I recommend studying the hardware user's manual and reviewing the "R_Config_SCI1_IIC_Master_Send" and related functions. Rewrite these functions to gain direct control of stop conditions and eliminate automatic stop conditions. 

    meanwhile, if you have questions don't hesitate to reach out here. 
     

    Regards, 
    Hossein.

    If this or any other user's response answers your concern, kindly verify the answer. Thank you!

    Renesas Engineering Community Moderator
    https://community.renesas.com/
    https://academy.renesas.com/
    en-support.renesas.com/.../

  • Hi,

    could you suggest I can modify the code used with smart configuration ?

    Br,

  • Hi,

    what is the correct baudrate that I need to use with M24256 chip.
    It seems slow the wrinting and the reading.

    Now I have 

    /* Set bit rate */

    SCI1.BRR = 0x19U;

    I modified the code inserting  this flag flag_e2read_pippuz and I set it to 1 when I need to write and put it to 0 when I need to read. The other part of the code is the code generated from Smart Configuration.

    The system seems slow.

    Please let me know if I am wrong or not.

     

    void r_Config_SCI1_receive_interrupt(void)

    {

    volatile uint8_t dummy;

    if (0U == SCI1.SISR.BIT.IICACKR)

    {

    if (_80_SCI_IIC_TRANSMISSION == g_sci1_iic_transmit_receive_flag)

    {

    if (g_sci1_tx_count > 0U)

    {

    SCI1.TDR = *gp_sci1_tx_address;

    gp_sci1_tx_address++;

    g_sci1_tx_count--;

    }

    else

    {

    if(flag_e2read_pippuz == 1)

    {

    /* Generate stop condition */

    g_sci1_iic_cycle_flag = _00_SCI_IIC_STOP_CYCLE;

    R_Config_SCI1_IIC_StopCondition();

    }

    }

    }

    else if (_00_SCI_IIC_RECEPTION == g_sci1_iic_transmit_receive_flag)

    {

    if (0U == SCI1.SIMR2.BIT.IICACKT)

    {

    if (g_sci1_rx_length > g_sci1_rx_count)

    {

    *gp_sci1_rx_address = SCI1.RDR;

    gp_sci1_rx_address++;

    g_sci1_rx_count++;

    }

    }

    else

    {

    dummy = SCI1.RDR;

    }

    if (0U == g_sci1_rx_count)

    {

    if(1U == g_sci1_rx_length)

    {

    SCI1.SIMR2.BIT.IICACKT = 1U;

    }

    else

    {

    SCI1.SIMR2.BIT.IICACKT = 0U;

    SCI1.SCR.BIT.RIE = 1U;

    }

    }

    else if (g_sci1_rx_length == (g_sci1_rx_count + 1))

    {

    SCI1.SIMR2.BIT.IICACKT = 1U;

    }

    else

    {

    /* Do nothing */

    }

    /* Write dummy */

    SCI1.TDR = 0xFFU;

    }

    else

    {

    /* Do nothing */

    }

    }

    else

    {

    /* Generate stop condition */

    g_sci1_iic_cycle_flag = _00_SCI_IIC_STOP_CYCLE;

    R_Config_SCI1_IIC_StopCondition();

    }

    }

    Br,

Reply
  • Hi,

    what is the correct baudrate that I need to use with M24256 chip.
    It seems slow the wrinting and the reading.

    Now I have 

    /* Set bit rate */

    SCI1.BRR = 0x19U;

    I modified the code inserting  this flag flag_e2read_pippuz and I set it to 1 when I need to write and put it to 0 when I need to read. The other part of the code is the code generated from Smart Configuration.

    The system seems slow.

    Please let me know if I am wrong or not.

     

    void r_Config_SCI1_receive_interrupt(void)

    {

    volatile uint8_t dummy;

    if (0U == SCI1.SISR.BIT.IICACKR)

    {

    if (_80_SCI_IIC_TRANSMISSION == g_sci1_iic_transmit_receive_flag)

    {

    if (g_sci1_tx_count > 0U)

    {

    SCI1.TDR = *gp_sci1_tx_address;

    gp_sci1_tx_address++;

    g_sci1_tx_count--;

    }

    else

    {

    if(flag_e2read_pippuz == 1)

    {

    /* Generate stop condition */

    g_sci1_iic_cycle_flag = _00_SCI_IIC_STOP_CYCLE;

    R_Config_SCI1_IIC_StopCondition();

    }

    }

    }

    else if (_00_SCI_IIC_RECEPTION == g_sci1_iic_transmit_receive_flag)

    {

    if (0U == SCI1.SIMR2.BIT.IICACKT)

    {

    if (g_sci1_rx_length > g_sci1_rx_count)

    {

    *gp_sci1_rx_address = SCI1.RDR;

    gp_sci1_rx_address++;

    g_sci1_rx_count++;

    }

    }

    else

    {

    dummy = SCI1.RDR;

    }

    if (0U == g_sci1_rx_count)

    {

    if(1U == g_sci1_rx_length)

    {

    SCI1.SIMR2.BIT.IICACKT = 1U;

    }

    else

    {

    SCI1.SIMR2.BIT.IICACKT = 0U;

    SCI1.SCR.BIT.RIE = 1U;

    }

    }

    else if (g_sci1_rx_length == (g_sci1_rx_count + 1))

    {

    SCI1.SIMR2.BIT.IICACKT = 1U;

    }

    else

    {

    /* Do nothing */

    }

    /* Write dummy */

    SCI1.TDR = 0xFFU;

    }

    else

    {

    /* Do nothing */

    }

    }

    else

    {

    /* Generate stop condition */

    g_sci1_iic_cycle_flag = _00_SCI_IIC_STOP_CYCLE;

    R_Config_SCI1_IIC_StopCondition();

    }

    }

    Br,

Children