Hi,
I am trying to read and write eeprom M24256.
I have used smart configuration but I am not able to read data in random address read.
Datasheet related eeprom said:
Random Address Read:
A dummy write is performed to load the address into the address counter. Then, without sending STOP condition, the master sends another START condition, and repeats the Device Select Code, with the RW bit set to 1. The memory acknowledges this, and outputs hte contents of the adressed byte. The master must not acknowledge the byte output, and terminates the transfer with stop condition.
Could you indicate to me how can manage this situation ?
Br,
Dear Lucaodex, I investigated that, and here's the result:Please follow the below project and test if it works on M24256. - When adding I2C master mode, use RIIC0
-In the "Config_RIIC0_user.c" file, declare an extern volatile _Bool flag, and make the below changes to the file.
-Main.c file:
/*********************************************************************** * * FILE : RX66N_IIC_EEPROM_Interfacing.c * DATE : 2024-03-28 * DESCRIPTION : Main Program * * NOTE:THIS IS A TYPICAL EXAMPLE. * ***********************************************************************/ #include "r_smc_entry.h" //Define the chip's address #define E1 0 //E1 pin logic #define E2 0 //E2 pin logic #define E3 0 //E3 pin logic #define B7_4_ADDR 0xA //Memory access address void M24xx_read_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* byte_buffer); void M24xx_write_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* const byte_data); void main(void); volatile _Bool IIC_transmission_end;//IIC bus busy state indicator uint8_t rx_buffer[10]; uint8_t tx_buffer[10] = {0xAA}; uint16_t memory_address = 0xFF;//An arbitrary address of the memory void main(void) { const uint8_t device_address = (B7_4_ADDR<<3 | E3<<2 | E2<<1 |E1);//Calculate and store the address of the chip R_Config_RIIC0_Start();//RIIC0 Initialization while (1) { M24xx_write_byte_random(device_address,&memory_address,&tx_buffer[0]);//save a byte to corresponding memory address R_BSP_SoftwareDelay(10, BSP_DELAY_MILLISECS); M24xx_read_byte_random(device_address,&memory_address,rx_buffer);//Fetch a byte from corresponding memory address R_BSP_SoftwareDelay(10, BSP_DELAY_MILLISECS); } } /* * Function: read a single byte from an arbitrary address * inputs: Device's address ,16bit address of the memory to be read,Function pointer to the data buffer * output: nothing */ void M24xx_read_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* byte_buffer){ //Divide 16bit address into two bytes uint8_t addr[2]; addr[0] = (uint8_t) ((*address) >> 8); addr[1] = *address; IIC_transmission_end = 0;//Reset IIC bus free flag R_Config_RIIC0_Master_Send_Without_Stop(device_address,(uint8_t*)addr, 2);//Send address to chip while(IIC_transmission_end == 0);//Wait for the data to be sent IIC_transmission_end = 0;//Reset IIC bus free flag R_Config_RIIC0_Master_Receive(device_address, byte_buffer, 1);//Retrieve the byte from the memory while(IIC_transmission_end == 0);//Wait for the bus to be free } /* * Function: write a single byte on an arbitrary address * inputs: Device address ,16bit address of the memory to be written,Function pointer to the data buffer * output: nothing */ void M24xx_write_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* const byte_data){ //Combine address and data to be send to the IC uint8_t data[3]; data[0] = (uint8_t) ((*address) >> 8); data[1] = *address; data[2] = *byte_data; R_Config_RIIC0_Master_Send(device_address,(uint8_t*)data, 3);//Send address and corresponding data to the chip } Now you probably can communicate with the chip properly. it obeys the Read/Write Sequence provided by the M24256 datasheet. The 0xAA value will be written to the 0xFF address of the chip, then you should be able to retrieve that data with the Random Read function.I hope you'll find it useful. don't hesitate to ask for clarification if you need it.
/*********************************************************************** * * FILE : RX66N_IIC_EEPROM_Interfacing.c * DATE : 2024-03-28 * DESCRIPTION : Main Program * * NOTE:THIS IS A TYPICAL EXAMPLE. * ***********************************************************************/ #include "r_smc_entry.h" //Define the chip's address #define E1 0 //E1 pin logic #define E2 0 //E2 pin logic #define E3 0 //E3 pin logic #define B7_4_ADDR 0xA //Memory access address void M24xx_read_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* byte_buffer); void M24xx_write_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* const byte_data); void main(void); volatile _Bool IIC_transmission_end;//IIC bus busy state indicator uint8_t rx_buffer[10]; uint8_t tx_buffer[10] = {0xAA}; uint16_t memory_address = 0xFF;//An arbitrary address of the memory void main(void) { const uint8_t device_address = (B7_4_ADDR<<3 | E3<<2 | E2<<1 |E1);//Calculate and store the address of the chip R_Config_RIIC0_Start();//RIIC0 Initialization while (1) { M24xx_write_byte_random(device_address,&memory_address,&tx_buffer[0]);//save a byte to corresponding memory address R_BSP_SoftwareDelay(10, BSP_DELAY_MILLISECS); M24xx_read_byte_random(device_address,&memory_address,rx_buffer);//Fetch a byte from corresponding memory address R_BSP_SoftwareDelay(10, BSP_DELAY_MILLISECS); } } /* * Function: read a single byte from an arbitrary address * inputs: Device's address ,16bit address of the memory to be read,Function pointer to the data buffer * output: nothing */ void M24xx_read_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* byte_buffer){ //Divide 16bit address into two bytes uint8_t addr[2]; addr[0] = (uint8_t) ((*address) >> 8); addr[1] = *address; IIC_transmission_end = 0;//Reset IIC bus free flag R_Config_RIIC0_Master_Send_Without_Stop(device_address,(uint8_t*)addr, 2);//Send address to chip while(IIC_transmission_end == 0);//Wait for the data to be sent IIC_transmission_end = 0;//Reset IIC bus free flag R_Config_RIIC0_Master_Receive(device_address, byte_buffer, 1);//Retrieve the byte from the memory while(IIC_transmission_end == 0);//Wait for the bus to be free } /* * Function: write a single byte on an arbitrary address * inputs: Device address ,16bit address of the memory to be written,Function pointer to the data buffer * output: nothing */ void M24xx_write_byte_random(uint8_t const device_address,uint16_t* const address, uint8_t* const byte_data){ //Combine address and data to be send to the IC uint8_t data[3]; data[0] = (uint8_t) ((*address) >> 8); data[1] = *address; data[2] = *byte_data; R_Config_RIIC0_Master_Send(device_address,(uint8_t*)data, 3);//Send address and corresponding data to the chip }
Kind regards, Hossien.
If this or any other user's response answers your concern, kindly verify the answer. Thank you!
Renesas Engineering Community Moderatorhttps://community.renesas.com/https://academy.renesas.com/en-support.renesas.com/.../
I have this configuration for the RX64M, so I have different pin.Can I use your suggestion changing the port or it is not possible ?
I have changed these conf inside:
void R_Config_RIIC01_Create(void)
{
....
/* Set SCL0 pin */
MPC.P30PFS.BYTE = 0x0FU;
PORT3.PMR.BYTE |= 0x01U;
/* Set SDA0 pin */
MPC.P26PFS.BYTE = 0x0FU;
PORT2.PMR.BYTE |= 0x40U;
.....
}