Using Renesas Flash Programmer with RX113 Starter Kit

Hi!

I want to use the Renesas Flash Programmer with the RX113 Starter Kit to donwload my program.
As far as I understand, I simply must put the MCU from Single Chip Mode to USB Boot Mode by setting SW4 to ON/ON, so that MD and UB (P14) are grounded, connect my PC to USB Port USB0_2, and then turn power on.

Bu when I do this, no device is detected by my PC. Using the Flash Progammer with an RX62 MCU works fine, it detecs a "Generic Boot USB Direct" device.

Do I need to connect to the USB Standard Type A connector instead of the Mini USB port? - But as I interprete the schematics, these share the same signals?

Thank you!

Parents Reply Children
No Data