e2 studio version: 2024-07
On Windows
Hi,
In the Software component configuration I am now unable to use the "Download and import sample projects". When I select this for a component and click; the Application Notes tab opens but no document is download this seems to have stopped working with the upgrade to 2024-07.
Regards
Hello,
Can you share a screenshot from e2studio?
For what module/driver do you try to download sampe project?
Regards,
AL_Renesas
It seems that you are right.
We will check it internally and iform you.
I was informed that this may be a web problem.
Also, it is under investigation, but for now, I cannot tell when will be fixed.
I will keep you informed, if I have any news.
I just got a new computer at the end of 2024 and updated the e2_studio to 2024-10. I just opened an existing project and it wanted to update the components. when I did the r_flash_rx was one of the components that updated and is shown on the overview information however it is missing in the project explorer after generating the project. is this possibly a problem related to one in this thread?