Download and import sample projects inComponent configuration

e2 studio version: 2024-07

On Windows

Hi,

In the Software component configuration I am now unable to use the "Download and import sample projects". When I select this for a  component and click; the Application Notes tab opens but no document is download this seems to have stopped working with the upgrade to 2024-07.

Regards

Parents Reply
  • I just got a new computer at the end of 2024 and updated the e2_studio to 2024-10. I just opened an existing project and it wanted to update the components. when I did the r_flash_rx was one of the components that updated and is shown on the overview information however it is missing in the project explorer after generating the project. is this possibly a problem related to one in this thread?  

Children
No Data