Motor control programming problem

Hello everyone,

I'm using a control board (RTK0EMX870C00000BJ) with an RX66T chip.

I've burned the induction motor control program from the website (Vector Control of Three-Phase Induction Motor Used in Driving a Pump RX66T Implementation Rev.1.10 - Sample Code) onto it.

I'm inputting a 3-phase sinusoidal signal from a signal generator to pins P40, P41, and P42.

When I test to see if these three current signals are being received in Renesas Motor Workbench, I find that the positive half-cycle of the signals is being cut off.I'm wondering if this is related to the values of g_f4_offset_iu, g_f4_offset_iv, and g_f4_offset_iw in the program, or if there's another reason. Does anyone know what might be causing this?




Regards,

RR

Parents Reply Children
No Data