Chip Select pin in SPI communication (RX72N)

Hello,

I'm working on communicating with a Pmod CAN controller connected to the CN5 (Pmod) port of the RX72N Envision Kit. I'm currently using the SCI/SCIF Clock Synchronous Mode to send and receive messages to the Pmod CAN controller. The MCP25625 integrated in the Pmod CAN controller requires the CS pin to be LOW before initiating a SPI communication, and then to return it to HIGH when the communication ends.

The thing is, the CS pin in the MCP25625 is mapped to the pin 52 in the RX72N Envision Kit, which is set to the SS2# (Slave Select 2) function in the Pin configuration section of Smart Configurator. This raises the following question:

The direction of pin 52 is fixed to Input, which is technically incorrect since the MCP25625 requires a variable LOW/HIGH signal on its CS pin, controlled by the RX72N's pin 52. Smart Configurator does not allow changing pin 52 to Input/Output mode nor it allows setting another pin for the task SS2#.

Parents
No Data
Reply
  • I got the answers for my questions:

    For question 1, turns out the MCP25625 starts acknowledging pulses whenever it receives the first pulse containing the message after the C̅S̅ pin goes down. So I ended up not needing this exact timing of lowering the C̅S̅ pin and immediately after (in the next clock pulse) sending the corresponding command I was talking about.

    For question 2, R_<Config_SCI0>_SPI_Master_Send_Receive manages the receiving part itself, meaning it doesn't matter when the slave responds, it always catches the message.

Children
No Data