boot loader project

Hi,

I'm trying to import the boot loader sample from this page: RX113-Starter-Kit - Renesas Starter Kit for RX113 | Renesas

but the latest e2 studio clearly doesn't see anything in the archive:

So how do I get an example of boot loader project for the rx113 ? because I'm expecting a linker script to be used, but only from the sample code structure, I'm not seeing it so I don't really get how it's done in the sample without opening and make a build happen.

Any help is appreciated.

have a good day

Parents
  • Hello,

    I am using E2 Studio 24-10.

    When I try to import the download sample codes, I select Import->Project  from Folder or Archive -> Select the downloaded Archive file.


    From your screenshot, I understood that tried to import the RX113 Renesas Starter Kit Sample Code for CS+ - R01AN2510EG0100. That is why E2 studio failed to import it.

    Please try again with the other provided Sample Code (R01AN2509EG0100)


    Thank you,
    Panos


Reply
  • Hello,

    I am using E2 Studio 24-10.

    When I try to import the download sample codes, I select Import->Project  from Folder or Archive -> Select the downloaded Archive file.


    From your screenshot, I understood that tried to import the RX113 Renesas Starter Kit Sample Code for CS+ - R01AN2510EG0100. That is why E2 studio failed to import it.

    Please try again with the other provided Sample Code (R01AN2509EG0100)


    Thank you,
    Panos


Children