adjusting the address/size of .istack, .ustack, and .data

I am developing on an RX651 using e2studio 2023 and GCC toolchain 8.3.0.202305 in a Windows 10 environment. 

I am to the point that I believe I have a stack overflow issue and need to increase the size of the allocated spaces.  I have adjusted the sections in earlier versions of e2studio, but I need an assist on locating the method of adjusting the sections of the 2023 edition.

Can anyone advise me?

Lane