IP Instance stops working SSP 1.7.12

HI.

In our proprietary board we have two ethernet interfaces (one for the lan and one for the wan). After a random time, it can be minutes or days, the interfaces stops working (mainly the wan that has telnet server). When interfaces crash, they don't even respond to ping.

I tried to debug the problem but unfortunately E2studio crashes after a while. What I have seen is that the IP Helper threads keep working even if they don't respond to the ping.

Now I have also enabled the traceX hoping to understand something. What do you think I should focus on?

Best Regards

Paolo

Parents
  • Hi Paolo,

    Same problem here with SSP 1.7.0. What i have found is that on a very intense traffic network, Ethernet stops to receive packets after a while. Note that my network has a lot of broadcast and multicast packets moving around (don't know why exactly...) it has cyclic peaks of thousands of packets per second.

    (As an additional reference to my network, note that ENC28J60 PHY from other device, also blocks due this intense traffic, but in this case is a known issue with that component)

    First, the problem has arise on a custom board, so I have moved to a PK-S5D9 board in order to see if the problem also happens, and yes it takes litle more time but it blocks at the end.

    So as it happens on both devices (with different PHY's) my conclusion is that there is something on SSP;

    What i've found:

    1 - When stops to reply to ping requests, data still is arriving to ethernet stack, you can see the packets updating memory pool area.


    2 - For an unknown reason, 'packet_type' seems to be corrupted so the new packets are not processed by the stack.

    From 'nx_renesas_synergy.c':1245

    /** Route the incoming packet according to its Ethernet type. */
    #ifdef FEATURE_NX_IPV6
    if (packet_type == NX_ETHERNET_IP || packet_type == NX_ETHERNET_IPV6)
    #else
    if (packet_type == NX_ETHERNET_IP)
    #endif
    {
    _nx_ip_packet_deferred_receive(nx_rec_ptr->ip_ptr, packet_ptr);
    }
    else if (packet_type == NX_ETHERNET_ARP)
    {
    _nx_arp_packet_deferred_receive(nx_rec_ptr->ip_ptr, packet_ptr);
    }
    else if (packet_type == NX_ETHERNET_RARP)
    {
    _nx_rarp_packet_deferred_receive(nx_rec_ptr->ip_ptr, packet_ptr);
    }
    else
    {
    /** Call the callback for unsupported packet type, if defined. */
    if ((NULL != nx_rec_ptr->p_callback_rec) && (NULL != nx_rec_ptr->p_callback_rec->nx_ether_unknown_packet_receive_callback))
    {
    nx_rec_ptr->p_callback_rec->nx_ether_unknown_packet_receive_callback(packet_ptr, packet_type);
    }
    else
    {
    /** If Ethernet header id invalid, release the packet. */
    nx_packet_release(packet_ptr); << ALWAYS GETTING HERE AFTER THE FAILURE
    }
    }
    return ;
    }

    I have seen on the forum, that more people has suffered this issue without get a clear solution.

    As a temporal workaround... is there any way to safely restart the ip stack?

    RENESAS PEOPLE: Note that i suspect that it only happen under a high network traffic environment so probably there is an unknown bug on the stack.

    Thaks!

    Oscar.

  • Hi Oscar.

    I also have a lot of broadcast and multicast traffic on my network. For the moment doing a dedicated VLAN seems to work without problems. I'll keep you up-to-date.

    Paolo

  • I do remember seeing a post about ethernet stop working :-

    https://renesasrulz.com/synergy/f/synergy---forum/15599/ethernet-reception-issue

    the user reported that resetting "bds_in_chain" at the end of the do..while() loop in the nx_rx_interrupt() function fixed the issue.

    The same user had a issue with the ethernet PHY hardware, on their own hardware.

  • Hi Jeremy.
    Unfortunately changing the variable reset didn't work in my case (if I understand it correctly). I made the following change:

    .Ethernet statistic

            Total packets sent: 166525
            Total bytes sent: 120059522
            Send packets dropped: 0
            Total packets received: 3065627
            Total bytes received: 8576741
            Received packets dropped: 2938960
            Received checksum errors: 0
            Invalid packets: 2
            Total fragments sent: 0
            Total fragments received: 0
            Packets pool (free/tot): 48/64
            Empty pool request: 0
            Empty pool suspensions: 0
            Invalid packets release: 0

    As you can see this time the Empty pool request was 0. The device that is on separate VLAN, for the moment, continues to work.

    Thanks

    Paolo

Reply
  • Hi Jeremy.
    Unfortunately changing the variable reset didn't work in my case (if I understand it correctly). I made the following change:

    .Ethernet statistic

            Total packets sent: 166525
            Total bytes sent: 120059522
            Send packets dropped: 0
            Total packets received: 3065627
            Total bytes received: 8576741
            Received packets dropped: 2938960
            Received checksum errors: 0
            Invalid packets: 2
            Total fragments sent: 0
            Total fragments received: 0
            Packets pool (free/tot): 48/64
            Empty pool request: 0
            Empty pool suspensions: 0
            Invalid packets release: 0

    As you can see this time the Empty pool request was 0. The device that is on separate VLAN, for the moment, continues to work.

    Thanks

    Paolo

Children