IP Instance stops working SSP 1.7.12

HI.

In our proprietary board we have two ethernet interfaces (one for the lan and one for the wan). After a random time, it can be minutes or days, the interfaces stops working (mainly the wan that has telnet server). When interfaces crash, they don't even respond to ping.

I tried to debug the problem but unfortunately E2studio crashes after a while. What I have seen is that the IP Helper threads keep working even if they don't respond to the ping.

Now I have also enabled the traceX hoping to understand something. What do you think I should focus on?

Best Regards

Paolo

Parents Reply
  • Hi.

    Unfortunately the -mno-unaligned-access option did nothing. Instead the device that has the separate network continues to work. Seeing as the changes didn't work out I'm back with the options and default code.

    In this case this shouldn't be a problem, as a separate network will be used with one or at most two devices connected, but on other implementations we plan to develop with these libraries it could be a problem.

    Best Regards

    Paolo

Children