HI.
In our proprietary board we have two ethernet interfaces (one for the lan and one for the wan). After a random time, it can be minutes or days, the interfaces stops working (mainly the wan that has telnet server). When interfaces crash, they don't even respond to ping.
I tried to debug the problem but unfortunately E2studio crashes after a while. What I have seen is that the IP Helper threads keep working even if they don't respond to the ping.
Now I have also enabled the traceX hoping to understand something. What do you think I should focus on?
Best Regards
Paolo
Paolo,
You're not alone on this. I'm also digging into Synergy code in order to find the root cause... but some help from RENESAS is welcome!
Best!
Oscar.
Hi Oscar-
Let us know if you find anything you want to ask about. You might consider starting a new thread if your environment is different enough from Paolo's that you think they might not be exactly the same....
Thanx, Warren
Hi all.
I confirm that isolating the network solved my problem, but this is still a problem that exists if using NetX on crowded networks.
Hi Warren,
Yes of course, I will open a separated thread with the proper SSP and enviroment.
My intention is also to be able to provide you a network capture which can cause the failure on your side.
Thank you in advance,