Hello,
I have a connection problem on AWS Cloud.I did create my Device on the account, as well as its shadow and embedded the 3 certificates: AmazonRootCA1.pem, .cert.pem, and .private.keyeach of these certificates is well recognized by the nx_secure_x509_certificate_initialize, nx_secure_tls_trusted_certificate_add and nx_secure_tls_local_certificate_add functions.Error 0x1007 is returned by the nxd_mqtt_client_secure_connect function after a correct nxd_mqtt_client_secure_connect and a first _nx_secure_tls_handshake_process as well. However, nx_secure_tls_session_receive ends up returning the error 0x56, (NX_NOT_CONNECTED).Note that my code was adapted for AWS because it originally worked for Cloud Azur. I could not use the AWS AE Cloud2 example code because it does not compile despite the SSP v1.7.8 version for which this code is intended.I hope someone here can help me?
Best Regards,
Eric F.