Hi,
I’m working with a S5D5 and I would like to create a bootloader which allow us to update the application in code flash using background operation. I see that on the S7G2 we can execute a bootloader in the first part of code flash memory in order to write the application in the second part of code flash memory :
But with the S5D5 doesn’t seem possible :
That’s the case ?
If not, how to proceed ? Will I need to create a bootstrap which copy my bootloader in ram ? Then execute the bootloader from RAM in order to update the application software in flash ?
Thanks you very much in advance.
Regards,
Hi Mota92i.We are looking into this and will get back to you.Thanks,Jayesh