Project for S7G2 with Azure IoT SDK(netxduo/addons/azure_iot)

We are planning to build a synergy project that connects to Azure Cloud. 

Since we are new to the synergy platform, we are looking for a sample project.

Can someone help us by sharing any sample project for the synergy platform(S7G2) that uses netxduo/addons/azure_iot/ ?

https://github.com/azure-rtos/netxduo/tree/068a9493ecd5af0024005ce695b992c4b172d6aa/addons/azure_iot 

Parents Reply
  • Check the settings of the used RMII-Channel and reset pin in the driver config. Additionally check the RMII pin configuration. They may be different on the S7-SK and the S5D9 Boards and I'm not sure if all the settings are migrated when you change the Board in the BSP-Tab.
    To check basic functionality and get a template for the right settings you can use a NetX example for the S7-SK, something with a Telnet-Server. Check the jumper settings on the SK.

    Pic is just an example, it does not necessarily shows the right settings for the S7-SK!

Children
No Data