Hello,
This is an example project based on e2studio 7.3. The e2 studio 2022-10 release note states this:
"The Synergy Software Platform version 1.x is no longer supported in e2 studio. The ability to manipulate the encrypted software platform source files is no longer included in the product. Please use an older product before 2022-10 to use these existing projects
You need an older e2studio version or manually port the source files/configurations etc into the latest e2studio project. In this case the example project would only be useful as a reference.
Hello AZ.