FAT on USB Mass Storage

Hi,

 

I would like to use the USB port to connect a memory stick and use it read/write files.

I have a old example here which uses "g_fx_media0 FileX on USB Mass Storage".

I am currently using SSP 1.2.1 and I am not finding this framework to add to my project.

 

Which framework should I use to achieve what I need?

Parents
  • Hi Mad River,

    You can find this stack in X-Ware > FileX > FileX on USB Mass Storage. In USBX on ux configuration make sure to set USBX Pool Memory Size to 65536 bytes and probably you may want to enable Auto Media Initialization in the top-level block of this stack.

    Regards,
    adboc
  • Hi adboc,

    I inserted the stack as you indicated.
    Tried to compile it and got these errors:

    ../src/synergy_gen/common_data.c: In function 'ux_host_init0':
    ../src/synergy_gen/common_data.c:299:59: error: 'SYNERGY_NOT_DEFINED_initialize' undeclared (first use in this function)
    SYNERGY_NOT_DEFINED_initialize, SYNERGY_NOT_DEFINED,
    ^
    ../src/synergy_gen/common_data.c:299:91: error: 'SYNERGY_NOT_DEFINED' undeclared (first use in this function)
    SYNERGY_NOT_DEFINED_initialize, SYNERGY_NOT_DEFINED,
    ^
    ../src/synergy_gen/common_data.c:300:59: error: 'UX_SYNERGY_CONTROLLER' undeclared (first use in this function)

     

     

    The function is that one:
    void ux_host_init0(void)
    {
    /** Register a USB host controller. */
    UINT status_g_ux_host_0 = ux_host_stack_hcd_register ((UCHAR*) "SYNERGY_NOT_DEFINED",
    SYNERGY_NOT_DEFINED_initialize, SYNERGY_NOT_DEFINED,
    UX_SYNERGY_CONTROLLER);
    if (UX_SUCCESS != status_g_ux_host_0)
    {
    g_ux_host_0_err_callback (NULL, &status_g_ux_host_0);
    }
    }

    What should I create to replace SYNERGY_NOT_DEFINED_initialize, SYNERGY_NOT_DEFINED and UX_SYNERGY_CONTROLLER?

     

     

     

    EDIT:

    I saw this is new content from 1.2.1.

    The only examples I could find are using 1.2.0.

    Is there any examples of how to use the FX on USB in the new 1.2.1? (Or at least how to compile the auto-generated code)

     

  • Mad River,

    You can set the timeout in the g_fx_media0 FileX on USB Mass Storage properties window. The default is 1000. If you want to hold off the thread until a memory stick is inserted, change the "Timeout ticks for Media Initialization" to 0xFFFFFFFF which is TX_WAIT_FOREVER.

    -Gary
  • Hi Gary,

    What if I don't want to block expecting to the memory stick be inserted?
    I would like to keep the application running and trigger a callback when the memory stick be inserted.

    I suppose that I can do it setting the auto-initialization of the fx file to "disabled".
    And do the following inside the triggered callback:

    /** Initialize the FileX Media Control Block g_fx_media0 for a USB Mass Storage device. */
    /** Get the pointer to a USBX Host Mass Storage Instance. */
    g_ux_host_class_storage0 = g_ux_new_host_storage_instance;

    /** Initialize the FileX Media Control Block g_fx_media0 for a USB Mass Storage device. */
    UINT err_g_fx_media0_get = ux_system_host_storage_fx_media_get (g_ux_new_host_storage_instance,
    &g_ux_host_class_storage0_media, &g_fx_media0_ptr);
    if (UX_SUCCESS != err_g_fx_media0_get)
    {
    g_fx_media0_err_callback_failed_to_get_fx_media (&g_fx_media0_ptr, &err_g_fx_media0_get);
    }

    Is my assumption correct?
  • Mad River,

    Yes, you can disable the auto init for g_fx_media0 and call it via the call back in USBX ux_host_change_callback to mount the stick. You will have to determine which device was just enumerated or de-enumerated in the callback.

    -Gary
  • Mad River,

     

    Here is an example of using the host change call back & event flags to init the media when its inserted.

    -Gary

    SK_S7_USB_MSC_Host_Example.zip

  • Hello Mad River,

    You can disable auto initialization and perform it yourself after the USB stick has been inserted. Please refer to the following example project for SK-S7 and SSP 1.2.0: s7_sk_ux_mass_host_1_2_0.zip. On SSP 1.2.0, you cannot call initialization from the insertion callback (init will block waiting for a semaphore that's placed only after the callback) so you'll need to use another semaphore to signal a thread to perform initialization.

    Regards

  • Hi everyone,

    I ran the example "USBX_Mass_Storage_Host_DK-S3A7" here.

    It worked, but not 100%. I repeatly inserted and removed the memory stick, and after some time it stop detecting the insertion.

     

    Anyway, I copied the thread shown in the example to my application.

    Not changed anything. Copied it as it is.

     

    The problem is that in my application the memory stick insertion is NEVER detected.

    In other words, the following code is never called:

    static UINT ux_system_host_change_function(ULONG event, UX_HOST_CLASS * host_class, VOID * instance) // THIS FUNCTION IS NEVER CALLED!
    {
         UINT status = UX_SUCCESS;
         SSP_PARAMETER_NOT_USED (event);
         SSP_PARAMETER_NOT_USED (host_class);
         SSP_PARAMETER_NOT_USED (instance);

        #if !defined(usb_host_plug_event_notification)
        /* Call user function back for USBX Host Class event notification. */
        status = usb_host_plug_event_notification (event, host_class, instance); // CALLS MY NOTIFICATION FUNCTION!

    }

     

    As I said, the example is based in the SSP 1.2.0 and I am using SSP 1.2.1. Is this change causing the problem I am facing?

    Or maybe something related to the DK-S3A7M2.0 or the DK-S3A7Bv2.0 (expansion board)? I am using the USB connector presented in the expansion board (DK-S3A7Bv2.0). Is any known issue with it?

     

     

     

    EDIT:

    More info about the problem.

    When I insert the memory stick, program goes to:

    void NMI_Handler (void)
    {

          if (1 == R_ICU->NMISR_b.SPEST)
         {
               /** MPU Stack Error interrupt is requested. */
               bsp_group_irq_call(BSP_GRP_IRQ_MPU_STACK);

               /** Clear MPU Stack error flag. */
               R_ICU->NMICLR_b.SPECLR = 1U;
    }

    }

     

     

    EDIT 2:

    I found the problem, but not the solution.

     

    In my project I have added the ThreadX Source component in order to alter the parameter "Timer Ticks Per Second".

    The memory stick detection (ux_system_host_change_function ()) is only called if I remove the ThreadX Source component from the project.

    Once I add the ThreadX Source component the ux_system_host_change_function() stop being called.

     

    Is it a known bug?

  • Hi!

    Have you double-checked that in Thread-X Source component properties you have Notify Callback property set to Enabled? By default, it is disabled, so it needs to be changed.

  • Hi,

    After enabling the "Notify Callbacks" the program goes to:

    void ux_v2_err_callback_internal(void * p_instance, void * p_data)
    {
    /** Suppress compiler warning for not using parameters. */
    SSP_PARAMETER_NOT_USED (p_instance);
    SSP_PARAMETER_NOT_USED (p_data);

    /** An error has occurred. Please check function arguments for more information. */
    BSP_CFG_HANDLE_UNRECOVERABLE_ERROR (0);
    }

    I really don't think that is the real problem cause.

    I added the ThreadX Source to the "USBX_Mass_Storage_Host_DK-S3A7.zip" example and it still works.

    Only my application crashes when using the ThreadX Source.

    Still don't know what to do...
  • Hi everyone,

    I discovered the cause of the problem.

    The USB doesn't work when setting the Optimization Level to None (-O0).

     

    I tested it in my own application and in the example provided by Renesas.

    Once I set the Optimization Level to None the USB stop working.

     

    The problem is that I need the Optimization Level set to None to my application work properly.

    What can I do?

  • Afaik, as long as the -O0 is only required for non-generatede code in your application, you could set -O0 for specific functions or whole blocks of code separate and leave the global settings at default.
Reply Children