HI,
I was using RGB565 earlier for displaying data and my RAM consumption was 580KB for 480x272 display. I want to limit my Graphics RAM to 300KB to 400KB Max, so i started using CLUT8,8bpp. I am using event as well. But i am getting window flashing for each update of timer of 1 second.
This issue was not happening in RGB565, 16 bpp. How to rectify this issue in CLUT8? Attached my program.
https://drive.google.com/file/d/0B2lqBLhAeTdLVmFjT2NtcW16RGc/view
Thanks,
Linto
DTDS
S7_SK_gx_clut8 (2).zip
Hi Linto,
CLUT should be also enabled in the configuration settings of the Display driver:
Please take a look at an example project:
S7_SK_gx_clut8.zip
Regards,adboc
Hi Phil,
Please find an example application and GUIX project for DK-S7G2 (SSP 1.3.3), it uses CLUT.
S7_DK_GUIX_CLUT_1_3_3.zip