CMake Error when import Project Example DA16200

Hi,

I tried to import a project for the Import TLS Server sample application (~/SDK/apps/common/examples/Network/TLS_Server/projects/da16200) , and 

I got  this error: "make: *** [makefile:230: all] Error 2" and make[1]: *** [src/subdir.mk:28: src/_write.o] Error 1.

I selected GNU Tools for ARM Embedded Processors (arm-none-eabi-gcc) and I checked that cmake.exe in the the PATH of C/C++ Project settings/Environment/Path.

1) PATH:

2) TOOLCHAIN:

                                                

3) Errors:

Parents Reply Children
No Data