Creating an Ubuntu Docker image for e2studios

I made a script which gets gcc from the release notes, gets e2 studios, copies in ssp 1.7.8 and then installs synergy from the command line. I run the script and it will generate a binary. It works great in ubuntu 20.04. 

When I try to run this inside of a docker container, i get totally different results. It will not build. Has anyone sucessfully generated a binary using e2studio from inside a docker container?

./e2studio \
--launcher.suppressErrors \
-nosplash \
-application org.eclipse.cdt.managedbuilder.core.headlessbuild \
-data worspace.headless \
-import "/sparkcharge/mcb/Production_v1" \
-build all \
-cleanBuild all \
-vmargs -Dcom.renesas.synergyLicenseFile="/home/orenderj/renesas_tools/temp/internal/projectgen/arm/licenses/SSP_License_Example_EvalLicense_20180725.xml"

Parents
  • Former Member
    0 Former Member

    Hello Orender,

    Our Development team saw this and they are considering looking into this as a special instruction notes or something.  Thank you for your input and it is always great when the community comes up with good solutions that others can use.

    Regards,

    Mike Quirk

  • I do have a working script in Ubuntu that will build a binary from a plain vanilla ubuntu machine and take any of my e2studios projects that are side by side with my script and build them. i assumed i could put this script onto my dockerfile, but it fails in a way that is difficult to determine as the errors are not very descriptive. the same command i wrote above, will fail on the command line, but it will generate 90% of the .o files for the project. i can finish the project manually if I then cd into the Debug or Release folder and "make all". I can also "make clean" and nuke the folder and "make all" again and it will succeed. I think I am getting down to the level where e2studio needs some requirements that I am not fulfilling inside my dockerfile even when it is in headless configuration. I suspect that it still looks for graphical components. If I install a jre, for example, things behave differently again. 

Reply
  • I do have a working script in Ubuntu that will build a binary from a plain vanilla ubuntu machine and take any of my e2studios projects that are side by side with my script and build them. i assumed i could put this script onto my dockerfile, but it fails in a way that is difficult to determine as the errors are not very descriptive. the same command i wrote above, will fail on the command line, but it will generate 90% of the .o files for the project. i can finish the project manually if I then cd into the Debug or Release folder and "make all". I can also "make clean" and nuke the folder and "make all" again and it will succeed. I think I am getting down to the level where e2studio needs some requirements that I am not fulfilling inside my dockerfile even when it is in headless configuration. I suspect that it still looks for graphical components. If I install a jre, for example, things behave differently again. 

Children