Hi,
I'm unable to debug in E2Studio.
"Error in Final launch sequence: GDB server failed to start"
Renesas e² studioVersion: 2023-10 (23.10.0)Build Id: R20231006-1456OS: Windows 10, v.10.0, x86_64 / win32Java vendor: Eclipse AdoptiumJava runtime version: 17.0.8+7Java version: 17.0.8
Debugger: E2Lite
Thanks,
Prashanth
Hello Prashanth,
Can you provide more information about the issue please?
1. What is the MCU you are using?
2. Did you test the e2Lite debugger on another PC? Does it work there?
3. Can you please provide the debugging log to see at what point the error happens?
Kind regards,
Sergey
If this response, or one provided by another user, answers your question, please verify the answer. Thank you!
Renesas Engineering Community Moderatorhttps://community.renesas.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/
Hi Sergey.
I'm using R5F104BA.
I can debug in CS+, but in e2studio getting Error in final launch sequence of debugger.
I have not tried in other PC.
Debug Log details-
GDB Server for Renesas targets.
Version 9.3.0.v20230925-111821 [e66fb063] (Sep 29 2023 00:42:49)
Starting server with the following options:
Raw options : C:\Users\bspem\.eclipse\com.renesas.platform_1598068615\DebugComp\\RL78\e2-server-gdb -g E2LITE -t R5F104BA -uConnectionTimeout= 30 -umFreq= 0 -usFreq= 0 -umClock= 1 -w 0 -usupplyVoltage= 0 -ucommMethod= 0 -usecurityID= 00000000000000000000 -usecurityIdSize 10 -upermitFlash= 1 -uuseWideVoltageMode= 1 -ueraseRom= 1 -uresetOnReload= 1 -ustopTimerEmu= 0 -ustopSerialEmu= 1 -umaskInternalResetSignal= 0 -umaskTargetResetSignal= 0 -n 0 -uverifyOnWritingMemory= 1 -uAllowRRMDMM= 0 -uRelayBreak= 0 -l -m -uCore= SINGLE_CORE|enabled|1|main -uSyncMode= async -uFirstGDB= main --english --gdbVersion= 7.2
Connecting to E2LITE, RL78 Target
GDBServer endian : little
Target power from emulator : Off
Starting target connection
Version Information:
RL78 E2 Lite Executor V4.10g [24 Oct 2022]
Finished target connection
Failed to create socket interface on port 0.
Disconnected from the Target Debugger.
The path in the debug command seems weird to me: "C:\Users\bspem\.eclipse\com.renesas.platform_1598068615\DebugComp\\RL78\e2-server-gdb". Can you check why is there a double backslash between the "DebugComp" and "RL78" folders? Is is a mistake in the command or does such folder really exist?
Thanks for the support.
Solved. Firewall causing the debugger to suspend.
Its working fine now.
Thank you for sharing your solution,
I will mark it as a verified answer to help the other people on this forum
Hi Emtron, I meet the same question as yours, how did you solve this issue?