Hi
i'm using e2 Studio
Version: 2024-01.1 (24.1.1)
Build Id: R20240125-1623
and have the rx compiler 3.06 installedI'm missing the memory views and other things in this menu which i had in older versions. How can i get them back?Regards
Hello,
You can try to use "Windows"-"Show View"-"Others..."
And in the opened window type what you need and open this view
Kind regards,
Sergey
If this response, or one provided by another user, answers your question, please verify the answer. Thank you!
Renesas Engineering Community Moderatorhttps://community.renesas.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/
i don't have these in this e2 studio version(in older version i had this tab)
Try to reinstall the e2studio. Maybe you missed some checkbox during installation. If the problem persists after this, I'll report your problem to the dev. team.
In e2 studio Version: 2024-01.1 (24.1.1) you can locate this view here.
Yep, but thats another view where you can view the contens of every memory adress.The other memory usage view is where you can see how much of your ROM is used
Same pull down as I talked about in the previous post but go all the way down and select other...
Then a new window will pop-up and you open the C/C++ tree and you will see it here