Renesas e2 Studio debugger not working

Hello,

I am using renesas E2 lite debugger for my custom RA4M1 MCU board.

I have connected my board to E2 lite debugger using the Serial Wire Debug (SWD) mode.

I have also selected correct MCU and E2 lite (ARM) debugger.

The code is compiling without any error (there are multiple warnings, which I am ignoring as of now).

when I am trying to launch the debug configuration I am getting the below error:-

After getting this error I tried to ask to chatgpt for some answer it said try to copy the folder from a working machine and paste it in the error location. for some reason it worked and I could use debug window to monitor expressions, but when I tried to pause the debugger use step into button the debugger collapsed and exited .

 I created one more project ( copy of the previous project ) and when I tried to launch that project for debug I got this error.

After spending some time, what I have understood is that the E2 studio is not generating .sbd for the projects, where as the previous project was readily imported and it already had a .sbd file and because I copy pasted that folder from the working machine it worked on my machine too. 

please suggest and help me do something about it.

My Debug Configuration:-

please let me know if more details are required I will be happy to share and assist.

Regards,

Sufyan