Hello,
I am using renesas E2 lite debugger for my custom RA4M1 MCU board.
I have connected my board to E2 lite debugger using the Serial Wire Debug (SWD) mode.
I have also selected correct MCU and E2 lite (ARM) debugger.
The code is compiling without any error (there are multiple warnings, which I am ignoring as of now).
when I am trying to launch the debug configuration I am getting the below error:-
After getting this error I tried to ask to chatgpt for some answer it said try to copy the folder from a working machine and paste it in the error location. for some reason it worked and I could use debug window to monitor expressions, but when I tried to pause the debugger use step into button the debugger collapsed and exited .
I created one more project ( copy of the previous project ) and when I tried to launch that project for debug I got this error.
After spending some time, what I have understood is that the E2 studio is not generating .sbd for the projects, where as the previous project was readily imported and it already had a .sbd file and because I copy pasted that folder from the working machine it worked on my machine too.
please suggest and help me do something about it.
My Debug Configuration:-
please let me know if more details are required I will be happy to share and assist.
Regards,
Sufyan