R9A02G021 jlinkexe error "Could not connect to the trget device"

Hi,

I ordered two of these boards. I used JLinkExe to download code to them and to debug programs on them.

JLinkExe no longer works with either board. I get the same error from both boards when trying to connect to them. Here are the messages that I get from JLinkExe:

Connecting to target via cJTAG
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 339us
Could not measure total IR len. TDO is constant high.
Failed to identify target. Resetting via Reset pin and trying again.
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 29us
TotalIRLen = 5, IRPrint = 0x05
JTAG chain detection found 1 devices:
 #0 Id: 0x00000001, IRLen: 05, Unknown device
Debug architecture:
  RISC-V debug: 0.13
  AddrBits: 14
  DataBits: 32
  IdleClks: 4
Memory access:
  Via system bus: No
  Via ProgBuf: Yes (8 ProgBuf entries)
  Via abstract command (AAM): May be tried as last resort
DataBuf: 4 entries
  autoexec[0] implemented: Yes
Failed to temporarily halt core during identification
Attaching to core failed. Trying again with connect under reset (ndmreset-bit)
Memory access:
Detected: RV32 core
Temp. halting CPU for for feature detection...
CPU could not be halted
Connect failed. Resetting via Reset pin and trying again.
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 11us
TotalIRLen = 5, IRPrint = 0x05
JTAG chain detection found 1 devices:
 #0 Id: 0x00000001, IRLen: 05, Unknown device

****** Error: Timeout while waiting for core to halt after reset and halt request
Specific core setup failed.
Error occurred: Could not connect to the target device.

Did anyone else have these problems? Any ideas of how to fix this?

Thanks for any help

Parents Reply
  • I have not changed any jumper settings on either of the boards.

    Both are bricked and JLinkExe gives the same error for both boards:

    "****** Error: Timeout while waiting for core to halt after reset and halt request"
    Specific core setup failed.
    Error occurred: Could not connect to the target device.

    I get the same error using Linux / Mac OS / Windows.

    I wonder if there is a problem with these boards?

Children