Hello,
Please confirm the marking for AT25SL321-MBUE-T.
AB
UEC
. 2049
BR
Krzysztof
sorry for delay < caused by our migration>. We are checking this.
AB = A = Serial Flash P/Ns AT25DF, AT25DN, ST25SF and AT25SL. B = 32Mbit Density Code
UEC = This is a unique identifier for the LOT code / MFG code. Only the factory can decide this and verify 100% this is SL321 in DFN 4x3
. 2049 = cy 2020 & work week 49
We're checking the lot-code to make sure its SL321.
BR JE_REN
can confirm this is the SL321. Thanks JE_REN