AT25SF041B generate no SPI signal

Hi,

I have connected the Flash memory to a STM32G071 Nucleo board.

For example I try to read the manufacturer and device Id, but the chip don´t send an answer. I tried 3 chips but all with the same result.

!Hold and !WP are connected to VCC. 

!CS is controlled by the controller. 

Clock frequency is 0,5MHz. 

Any suggestion why i don´t get an answer from the chip?