Hi. I have 2 questions regarding the AT25SF041B:
Hi Lulu,When interfacing flash memory to MCU the currents flowing in or out of the I/O pins determine the correct logic levels.The parameters Vcc, IOL and IOH determine this. Since CS# and WP#(I/O2) are…
Hi Lulu,When interfacing flash memory to MCU the currents flowing in or out of the I/O pins determine the correct logic levels.The parameters Vcc, IOL and IOH determine this. Since CS# and WP#(I/O2) are I/O pins, their electrical characteristics are shown as I/O electrical characteristics in the datasheet table.The max current required to achieve the logic level 0 (LOW) in case of #CS is a sinking current of 100 μA.WP# is internally pulled-high does not always mean there is a resistor pulling it high.IOL and IOH are the numbers you look at.
Best regards,Renesas Electronics Online Support