AT25SF041B active current

Hi. I have 2 questions regarding the AT25SF041B:

  1. I'm looking for the active current for the AT25SF041B when CS# is asserted but no command is sent. The datasheet only mentions the active current for specific commands, but the waveforms show that the device starts consuming "active current" as soon as CS# is asserted. I would want to share the same line as CS# with a different device but would need to make sure I'm not drawing too much current when the line is asserted and no command is sent. 
  2. Also, the datasheet states that WP# is internally pulled high but does not provide any value for the pull-up. Is it possible to get the actual value of the pull-up?