Dear Renesas Team,
Could you provide me with the Verilog behavior model for 70261 SRAM?Thanks!
Best Regards,Jason Shih
The only models that we currently have are:
70261PF TQFP HSpice Model
70261PF TQFP IBIS Model
Hi OV_Renesas,
I apologize, but these two models cannot be used for Verilog verification. Could you please confirm if the control methods for this SRAM and the 7025L20PFGI are the same? If they are, can I use the Verilog model for the 7025L20PFGI that I obtained previously for simulation, or do I only need to modify the config.idt file? If modifications to the config.idt file is necessary, could you please assist me in adjusting it for the 70261?Thank you!
Hi Shih01,
I will check into this and let you know. ( ASI-1057 )
Dear Jason,Apologies for the delay.We are checking for the 70261 Verilog files and could not find it in the standard folder. We are now searching old archives. Best Regards,OV_Renesas
Hi,
Okay, thanks for your help!
Shiho1,
Our designer has confirmed that the 7025 Verilog model can be configured for use with the 70261 device. Please follow the instructions in the readme file, that should be sufficient for your needs.
7025U Verilog.zip
Thank you very much to your team. This will be very helpful to me.