Looking for step-up dc/dc converter with Vin 2.5V , Vout 30V

Hello Team,

I am looking for a boost converter with the following requirements :

Vin 2.5 To 4V

Vout >30V

power output 8W,

I did not manage to find any boost device that accepts Vin below 4.5V, could you please advise if we have anything to offer?

Thanks in advance.

Kind regards,

Shai

Parents Reply
  • Shai  shalom you   can use ISL97519A   with extrenal  Fet  for higher  voltage  choose a  fet  with 65-55v at least   see   explanation in the   datasheets make sure you  are  with in  the  chip correct   spec limitation of the chip  & run  ISIM simulation at 500kHz   any  if you have  questions  please call me  shabat shalom  koby

    Galberg Avnet Silica  Israel  :

Children