ISL81601 UPS with low voltage battery/capacitor

Hello!

I would like build a UPS with only 1 cell of Li-Ion battery (max. 4.2V) or supercapacitor (max. 2.7V). System bus would be 5V.

According to the datasheet the minimum voltage on Vin should be minimum 4.5V, so I can't use the Vin side of the dcdc converter for the battery, as discribed in "Design Considerations for a Bidirectional DC/DC Converter" white paper. 

Is it possible to  swap the sides, and use the Vout side of the controller for the battery (min. 0.8V is low enough), and Vin for the system bus?

Thanks for help in advance.

Br,

Zoltan

Parents
  • Hi, 

    What's your output /load requirement  (v& I). 

    Figure 3 shows the four-switch buck-boost converter operation modes and waveforms controlled by the ISL81601. When Vin is lower than Vout, it runs in boost mode, as shown in Figure 3C. When Vin is higher than Vout, it runs in buck mode, as shown in Figure 3A. When Vin is close to Vout, it runs in buck-boost (one cycle buck followed by one cycle boost) mode as shown in Figure 3B .   

    Also As per flow of charge & discharge . Vin  to Vout is buck converter  & Vout to Vin boost converter . If you connect battery at output side you will get boost voltage at input side . & vice versa.

    Thanks 

    AB 

  • Hi,

    Charge current is 3A, max. battery voltage is  between 4.2V and 2.7V. System current is 3A, system voltage is 5V.

    Br,

    Zoltan

  • Hi, 

    Can You share block diagram to understand more .

    Thanks 

    AB 

  • Hello!

    Here is the block diagram.

    Br,

    Zoltan

  • Hi, Zoli! Did you manage to solve this problem?
    Did you put the battery on the VIN side?

  • Hi,

    We have built the ups with ISL81401 with 12V system bus. It is charging the battery without any problem, but not doing the 12V from the battery, when  we are removing the power supply, so not working backwards. I have checked the mosfet gates, but there is no pulses in case of backwards direction.

    Any suggestion, what we have to check?

    Thanks for help in advance.

    Br,

    Zoltan

  • Hello, Zoli! I'm glad there is feedback.
    Now I have created a project 12V source - IS81601 - 4S7P battery from 10V-16V (the battery is hanging on the output of the microcircuit). I am waiting for the components and will include this board.
    Zoli, tell me the parameters of the circuit. Is the input of the microcircuit hanging on the main 12V line? and the battery is hanging on the output of the microcircuit?
    What kind of battery do you have? What is the battery voltage range?
    As I understand the operation of the circuit - (if the main 12V and the load are from the input side of the microcircuit, and the battery is on the output side) - then when the main 12V (at the input) disappears, you need to force the GM2 circuit to change the direction of energy (from the battery towards the main 12V). That is, you need to select a divider for the GM2 circuit slightly below 12V.

  • Hello Korg!

    Thanks for the answer.

    Yes, the input is connected to the main 12V line, and battery is to the output. Actually battery is a single LIFEPO4 one (2.5-3.6V), but can be upgraded to 2S or 3S. Instead of ISL81601 we have used ISL81401, as 40V limit is high enough. Ru is 620k, Rd is 47k, calculated voltage on input is 11.35V.

    On test  PCB we used 4 mosfet (Q1-Q4), but actually there are only 2 implemented (Q1 and Q2), as it is purily a buck converter (and boost in reverse direction). Q4 is shortcircuit, and Q3 is open.

    In reverse mode there is 2.8V on input side, battery is 3.2V,  LG1 is steady 0V, UG1 is steady 3.2V (tested on oscilloscope). It looks the controller relucting to do its job is the direction. There is no load on the system, only the multimeter.

    Br,

    Zoltan

  • Try playing (putting a variable resistor) on the FB-OUT divider. Create a condition where the Battery Voltage is higher than the FB-OUT setting
    With the correct bias of the current sense op amps in the ISL81401 controller, it can sense and control both positive and negative currents at both the input and output. This is important for reliable operation of a bidirectional DC/DC converter.
    A bidirectional DC/DC converter requires control of the input/output voltage and current.
    That is why it is important to be able to adjust the Input and Output voltage dividers.
    Can you send me a schematic of your project?

    [email protected]

  • Hi!

    Fortunatelly we could find the solution.

    Chip was in "DEM" mode (MODE pin was forced to "High"), which have  blocked the reverse mode.

    Actually we have a new problem. In reverse direction the output voltage is 11.3V. If we increase the load, around 0.9A, the voltage start to decrease significantly, at 1A it is only 9V.

    Battery voltage is 3.15V. What can be the problem?

    Br,

    Zoli

  • Hello! Interesting point. Your voltage drops under load, are you using only one battery? Additionally, install electrolytic capacitors on the output and input. Perhaps you do not have enough power from one battery?

Reply Children