Hi,
Does it support 1-Wire serial programming (TOOL0) or only dual-wire ? In this last case, which Tx/Rx pin is used (TxD0/RxD0 or TxD1/RxD1) ? What programming protocol does this chip support (from A to D) ?
The datasheet only talks about "TOOLRxD/TOOLTxD" mode (00H=Dual Wire mode) but theses pins are not defined.
Many thanks.
Best regards
i will check & come back to you
Thanks
Ab
In RAJ240080 use case, the flash memory programming mode uses only TOOL0 pin (and RESET pin).
Please refer the following picture.
AB
So the RAJ240080 should work with the Flash Programmer set to 1-Wire UART when selecting RL78 as microcontroller? For some reason I don't get any response.