RAA226110

Hello, I am working with the RAA226110 low-side gate driver component. I am encountering a weird issue. I am using this to drive two Ganfets in the design of a power supply. When testing the pcb board with the RAA226110 by itself, it works perfectly fine. The output of the board is a scaled down version of the input signal. As soon as I connect the gate driver pcb to the mosfet gates, the output signal messes up. If anyone has any insight on this issue it would be very helpful.

(Picture of expected waveform (orange) verus the ouput signal which is messed up (green))

(Picture of output (green) and voltage at pin 12 VDRV (orange)

Schematic of PCB for the  RAA226110 (isolated, without other power supply design components)

Parents
  • Thank you for your inquiry regarding the use of a GaN FET driver to drive a MOSFET. Here's a detailed explanation:

    It is generally not recommended to use a GaN FET driver to drive a MOSFET. While it may be technically possible with few hardware changes, there are several reasons why this is not ideal:

    Key Reasons:

    1. Gate Drive Voltage Requirements
    2. Gate Charge Differences
    3. Switching Speed and Timing
    4. Impedance Mismatch

    However, if you still prefer to use a MOSFET for any reason, several hardware modifications will be necessary. Please share the details of the MOSFET and detailed schematic you are using, and I will recommend the specific hardware changes needed to ensure proper operation.

    Regards,

    Avinash Kumar

Reply
  • Thank you for your inquiry regarding the use of a GaN FET driver to drive a MOSFET. Here's a detailed explanation:

    It is generally not recommended to use a GaN FET driver to drive a MOSFET. While it may be technically possible with few hardware changes, there are several reasons why this is not ideal:

    Key Reasons:

    1. Gate Drive Voltage Requirements
    2. Gate Charge Differences
    3. Switching Speed and Timing
    4. Impedance Mismatch

    However, if you still prefer to use a MOSFET for any reason, several hardware modifications will be necessary. Please share the details of the MOSFET and detailed schematic you are using, and I will recommend the specific hardware changes needed to ensure proper operation.

    Regards,

    Avinash Kumar

Children
No Data