RAA226110

Hello, I am working with the RAA226110 low-side gate driver component. I am encountering a weird issue. I am using this to drive two Ganfets in the design of a power supply. When testing the pcb board with the RAA226110 by itself, it works perfectly fine. The output of the board is a scaled down version of the input signal. As soon as I connect the gate driver pcb to the mosfet gates, the output signal messes up. If anyone has any insight on this issue it would be very helpful.

(Picture of expected waveform (orange) verus the ouput signal which is messed up (green))

(Picture of output (green) and voltage at pin 12 VDRV (orange)

Schematic of PCB for the  RAA226110 (isolated, without other power supply design components)