Hi,I've built a system around the ISL94202 that has an integrated battery pack (the cells/BMS circuit are not removeable once assembled). The first time the device is assembled it works okay because the batteries are connected to the BMS prior to any load being attached.However I'd ideally like to be able to put the device into a "Powerdown State" for long term storage. The problem that I have is that the load is not removeable so after reconnecting the charger the device is unable to transition from "Power-On Reset" to "Normal Operating Mode".
Is there any way to configure the ISL94202 to ignore the presence of a load for this state transition?
Alternatively I could place a FET in the discharge path that is controlled by the charger, to disconnect the load while a charger is present. Then the charger would just need to be connected long enough for the ISL94202 to reach "Normal Operating Mode", but this would require additional components.
Thanks,Errol