ISL94202 Reset/Reboot

I'm having an issue with ISL94202 where one of the cell voltages will be reported lower than it actually is. If the technicians desolder the pack and re-attach (effectively rebooting the chipset) the voltage will report correctly. Typically the voltage error is 100-150mV reporting 4000mV instead of the actual 4160mV

I'm looking for a method to power cycle the chipset without disconnecting power as its very time consuming to do in production.

Thank you,