This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Combining reverse operation and burst mode in ISL81601

Hello. 

Is it possible for ISL81601 to work in burst mode for light loads on Output, but also to allow reverse mode when voltage drop at Input occure? 

From what i understand:

- adding resistor from LG1 to PGND enables reverse mode, but disables burst mode 

- removing resistor from LG1 to PGND disables reverse mode, but enables burst mode 

 

I'm trying to use ISL81601 to build supercapacitor DC-UPS. Capacitors are on the output, powered system and power supply at the input. I would like ISL81601 to work in burst mode while the input power source is online and the capacitors are fully-charged and to switch to reverse mode in case of voltage drop at the input. 

Best Regards 

Dominik Bejma




[locked by: AK_Renesas at 12:55 (GMT 0) on 29 Oct 2024]