Hi,
We are current using D9053 for i.MX53 processor and want to change it to DA9063.
Does DA9063 support i.MX53? is the driver/configuration available in BSP QNX6.5?
Is DA9053 driver/configuration able to support DA9063 as well?
Thanks.
Hi Michael, I will get back to you in a while.
Regards,
Avinash Kumar
Which DA9053 OTP vision are you using for I.MX53?
The DA9063 can support the i.MX53 with OTP vision
Thanks
AB
can you pleae provide more details?
1. About DA9063, do you have linux configuraton/driver code which support i.MX53. and please send us the link.
2. is QNX (vison 6.5) supportING the DA9063 for i.MX53?
3. Is DA9053 configuration/driver code compatible with DA9063
There may be a DA9063 variant that has a suitable rail configuration for the i.MX53 but for same to get details
kindly submit a Technical Support ticket by going to our support portal from the following link: https://en-support.renesas.com
You will need to sign in with your company email address, and if you don't have an account you will need to register with one. https://www.renesas.com/register