ISL81801 Bi-Directional Operation

Hello, 

I have an application that allowing current flow in both directions in a buck/boost fashion.  It includes a battery and a charger/load.  I have a few questions related to this:

- Is it recommended to have the battery on the input side or the output side of the ISL81801 circuit?

- How does the ISL81801 regulate forward vs reverse current? The spec sheet isn't very clear on how it would know which way the current should flow. My application needs to regulate input CV/CC as well as output CV/CC (not all simultaneously), so how does the chip know what takes precendence? For example - if I need the battery voltage to stay at or below 30v, and the battery charge current to not go above 20A, how do I set the other CV/CC values so that the battery regulation is correct?

Please let me know if something is unclear or needs clarification.

Thank you in advance,

Ryan M.