Hello,
I want to design a buck/boost converter with Vin = 35-58V, Vout = 48V, and Iout = 21A. Can I design the desired circuit using the ISL81601 IC? Will the current value cause any issues?
Thank you in advance for your help.
Hi,
I'll get back to you shortly regarding your query.
Regards,
Avinash Kumar
The ISL81601 buck/boost converter offers a wide input voltage range from 4.5V to 60V and an output voltage range from 0.8V to 60V. The maximum output current, which depends on the external MOSFETs, can support 21A, making this IC a suitable choice for your design.
Regards,Avinash Kumar
Hello Avinash Kumar,
Thanks for your answer.
Regards.
Hello! Avinash Kumar!Please tell me what is the reason for the current limitation of 21A?I can take transistors that allow working at a current of 50A (for example IQDH29NE2LM5ATMA1 MOSFET N-CH 25V 75A PG-TSON-8).What is the reason for the current limitation in the ISL81601 microcircuit?
Hi Korg,
You can use a 50A-rated MOSFET with the ISL81601 without any inherent issues.
Thanks, and regards,
Thanks for the answer!Can you explain in more detail what limits the maximum current for ISL81601?
There are no such limits as the current depends on the MOSFET rating.