I have a question about the market performance of DA9131.Has DA9131 been sold for automotive use so far?I don't want to know the specific company name. (I understand that it cannot be disclosed.)I just want to know if DA9131 has been adopted for automotive use.
Hi,
I will be back with an update.
Thanks and regards,
Avinash Kumar
The DA9131 has been qualified for automotive use. Specifically, it is AEC-Q100 Grade 2 qualified, which ensures its suitability for automotive applications. This qualification means that the device has met the necessary requirements for operation in automotive environments, including temperature ranges from -40°C to +105°C.
Thanks, and regards,
Sorry. I'm asking if DA9131 has ever been used in a automotive.
What I want to know is the sales record.
Thanks, and regards.