About the market performance of DA9131

I have a question about the market performance of DA9131.
Has DA9131 been sold for automotive use so far?
I don't want to know the specific company name. (I understand that it cannot be disclosed.)
I just want to know if DA9131 has been adopted for automotive use.

Parents
  • Hi,

    The DA9131 has been qualified for automotive use. Specifically, it is AEC-Q100 Grade 2 qualified, which ensures its suitability for automotive applications. This qualification means that the device has met the necessary requirements for operation in automotive environments, including temperature ranges from -40°C to +105°C.

    Thanks, and regards,

    Avinash Kumar

Reply
  • Hi,

    The DA9131 has been qualified for automotive use. Specifically, it is AEC-Q100 Grade 2 qualified, which ensures its suitability for automotive applications. This qualification means that the device has met the necessary requirements for operation in automotive environments, including temperature ranges from -40°C to +105°C.

    Thanks, and regards,

    Avinash Kumar

Children