ISL91302BIIZ I2C Communication unable to establish using stm32 mcu

I am using STM32L496QGI6P mcu to communicate with the ISL91302BIIZ-TR5931 PMIC.

Following is my relevant code which uses i2c3 (pg7/pg8 pins on mcu for scl/sda), I am also initializing GPIO PE1 as EN pin for PMIC. I am at the end scanning the i2c3 bus to see if I can find any device but I am not able to get a communication on any of the I2C addresses.

else if(hi2c->Instance==I2C3)

{

/* USER CODE BEGIN I2C3_MspInit 0 */

/* USER CODE END I2C3_MspInit 0 */

/** Initializes the peripherals clock

*/

PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_I2C3;

PeriphClkInit.I2c3ClockSelection = RCC_I2C3CLKSOURCE_PCLK1;

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

{

Error_Handler();

}

__HAL_RCC_GPIOG_CLK_ENABLE();

/**I2C3 GPIO Configuration

PG7 ------> I2C3_SCL

PG8 ------> I2C3_SDA

*/

GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;

GPIO_InitStruct.Pull = GPIO_PULLUP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.Alternate = GPIO_AF4_I2C3;

HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

/* Peripheral clock enable */

__HAL_RCC_I2C3_CLK_ENABLE();

/* USER CODE BEGIN I2C3_MspInit 1 */

/* USER CODE END I2C3_MspInit 1 */

}

void I2C3_ScanBus(void) {

printf("Scanning I2C3 bus...\n");

//Reinit_I2C3();

//__HAL_RCC_I2C3_CLK_ENABLE();

for (uint8_t addr = 0x03; addr <= 0x77; addr++) {

// Shift address to 8-bit form (HAL expects 8-bit address)

if (HAL_I2C_IsDeviceReady(&hi2c3, addr << 1, 2, 10) == HAL_OK) {

cmis_page0[0] = addr;

}

HAL_Delay(10);

}

printf("Scan complete.\n");

}


int main(void)

{

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

/* MCU Configuration--------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

/* USER CODE BEGIN Init */

/* USER CODE END Init */

/* Configure the system clock */

SystemClock_Config();

PeriphCommonClock_Config();

/* USER CODE BEGIN SysInit */

/* USER CODE END SysInit */

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_I2C4_Init();

MX_I2C2_Init();

MX_ADC1_Init();

MX_ADC2_Init();

MX_ADC3_Init();

__HAL_RCC_SPI1_CLK_ENABLE();

MX_SPI1_Init();

__HAL_RCC_I2C2_CLK_ENABLE();

__HAL_RCC_I2C4_CLK_ENABLE();

HAL_GPIO_WritePin(GPIOG, GPIO_PIN_6, GPIO_PIN_RESET);

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_RESET);

HAL_Delay(1000);

HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_SET);

HAL_Delay(1000);

MX_I2C3_Init();

__HAL_RCC_I2C3_CLK_ENABLE();

I2C3_ScanBus();

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

/** Configure the main internal regulator output voltage

*/

if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)

{

Error_Handler();

}

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;

RCC_OscInitStruct.MSIState = RCC_MSI_ON;

RCC_OscInitStruct.MSICalibrationValue = 0;

RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

Error_Handler();

}

}

/**

* @brief Peripherals Common Clock Configuration

* @retval None

*/

void PeriphCommonClock_Config(void)

{

RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

/** Initializes the peripherals clock

*/

PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC;

PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_PLLSAI1;

PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_MSI;

PeriphClkInit.PLLSAI1.PLLSAI1M = 1;

PeriphClkInit.PLLSAI1.PLLSAI1N = 8;

PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV2;

PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV2;

PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV2;

PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_ADC1CLK;

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

{

Error_Handler();

}

}

static void MX_I2C3_Init(void)

{

/* USER CODE BEGIN I2C3_Init 0 */

/* USER CODE END I2C3_Init 0 */

/* USER CODE BEGIN I2C3_Init 1 */

/* USER CODE END I2C3_Init 1 */

hi2c3.Instance = I2C3;

hi2c3.Init.Timing = 0x10030D09;

hi2c3.Init.OwnAddress1 = 0;

hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

hi2c3.Init.OwnAddress2 = 0;

hi2c3.Init.OwnAddress2Masks = I2C_OA2_NOMASK;

hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

if (HAL_I2C_Init(&hi2c3) != HAL_OK)

{

Error_Handler();

}

/** Configure Analogue filter

*/

if (HAL_I2CEx_ConfigAnalogFilter(&hi2c3, I2C_ANALOGFILTER_ENABLE) != HAL_OK)

{

Error_Handler();

}

/** Configure Digital filter

*/

if (HAL_I2CEx_ConfigDigitalFilter(&hi2c3, 0) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN I2C3_Init 2 */

//HAL_I2CEx_EnableFastModePlus(I2C_FASTMODEPLUS_I2C3);

/* USER CODE END I2C3_Init 2 */

}

static void MX_GPIO_Init(void)

{

/* USER CODE BEGIN MX_GPIO_Init_1 */

/* USER CODE END MX_GPIO_Init_1 */

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOE_CLK_ENABLE();

__HAL_RCC_GPIOC_CLK_ENABLE();

__HAL_RCC_GPIOF_CLK_ENABLE();

__HAL_RCC_GPIOG_CLK_ENABLE();

HAL_PWREx_EnableVddIO2();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOD_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

GPIO_InitStruct.Pin = GPIO_PIN_1;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

Can you help to check if the initialization sequence for PMIC is correct and if I am missing setting anything on PMIC before which I will be able to communicate with PMIC using I2C.

Parents Reply
  • Hello Avinash,

    Thanks for the reply. Below is the schematic which we are using:

    In my code, I follow the following flow: HAL Init->I2C3 Init->EN pin High->wdog reset low->scan for PMIC (or) HAL Init->I2C3 Init->wdog reset low->EN pin High->scan for PMIC. I have put some delay between the calls. But, I am still unable to detect the PMIC using I2C.

Children