Hi,
I have a problem about programming QSPI flash with either e2 studio or .bat file command system. I use Stream It kit.
it gives result succesfull download to QSPI flash but application not running.
also I couldn't see any drivers and sample example for SPI multi IO bu controller.
any idea about these?
thanks.
Hi yzcifci,
Have you already solved this problem? Please wait until RZ experts respond to your issue. Thank you.
JBRenesasRulz Forum Moderator
https://renesasrulz.com/https://academy.renesas.com/https://en-us.knowledgebase.renesas.com/
tried settings but nothing changed. images above is stream it kit that ı use, thanks
right, SPANSION chip mounted on board, I can not program the QSPI chip ; so if I edited the correct settings , how will I download to the flash ?. chip on board is R7S7210121VC .
I see that qspi communication is ok on the scope. But erasing the device is not succesfull. I doubt that qspi spansion chip may be in a protected state that I can not erase the device, So I can not erase or program the device. J link flasher says erasing ok but when I look in the memory browser e2 studio looks erase (memory area is different from 0xff) unsuccesfull.