Hi,
I have a problem about programming QSPI flash with either e2 studio or .bat file command system. I use Stream It kit.
it gives result succesfull download to QSPI flash but application not running.
also I couldn't see any drivers and sample example for SPI multi IO bu controller.
any idea about these?
thanks.
I see that qspi communication is ok on the scope. But erasing the device is not succesfull. I doubt that qspi spansion chip may be in a protected state that I can not erase the device, So I can not erase or program the device. J link flasher says erasing ok but when I look in the memory browser e2 studio looks erase (memory area is different from 0xff) unsuccesfull.
In datasheet says that Advanced Sector Protection password method can be permanently enabled and this register bit is one time programmable, then device requires password to read or write, doesn't it?