docker run makes kernel into panic mode with smarc-rzg2lc

I am following this renesas guide for yocto image installation :https://www.renesas.com/us/en/document/mas/rzg2-group-yocto-recipe-start-guide-vlp-v300? r=1467986 and I have added docker in that image.

My board functionality is as below.
Kernel: 5.10.83-cip1+gitAUTOINC+e52825e45b
Docker version 19.03.8-ce, build afacb8b7f0
Installed docker in yocto using this command: MACHINE_FEATURES_append = " docker"

root@oldsilicon:~#sudo systemctl enable docker
root@oldsilicon:~#sudo systemctl start docker
root@oldsilicon:~# docker pull helloworld
root@oldsilicon:~# docker run hello-world
[ 343.095177] IPv6: ADDRCONF(NETDEV_CHANGE): veth0e6d0a7: link becomes ready
[ 343.104819] IPv6: ADDRCONF(NETDEV_CHANGE): vethe61d7c2: link becomes ready
[ 343.121967] docker0: port 1(veth0e6d0a7) entered blocking state
[ 343.129042] docker0: port 1(veth0e6d0a7) entered disabled state
[ 343.135825] device veth0e6d0a7 entered promiscuous mode
[ 343.142104] kauditd_printk_skb: 29 callbacks suppressed
[ 343.142109] audit: type=1700 audit(1675680946.586:44): dev=veth0e6d0a7 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
[ 343.154381] docker0: port 1(veth0e6d0a7) entered blocking state
[ 343.165400] docker0: port 1(veth0e6d0a7) entered forwarding state
[ 343.174487] IPv6: ADDRCONF(NETDEV_CHANGE): docker0: link becomes ready
[ 343.663141] cgroup: cgroup: disabling cgroup2 socket matching due to net_prio or net_cls activation
[ 343.966632] Unable to handle kernel paging request at virtual address 000f02fa0202012a
[ 343.967549] Unable to handle kernel paging request at virtual address 006b636f642f6dbe
[ 343.974630] Mem abort info:
[ 343.974643] ESR = 0x96000004
[ 343.982729] Unable to handle kernel paging request at virtual address 000102080102020a
[ 343.985329] EC = 0x25: DABT (current EL), IL = 32 bits
[ 343.988363] Mem abort info:
[ 343.996245] SET = 0, FnV = 0
[ 344.001528] ESR = 0x96000004
[ 344.004307] EA = 0, S1PTW = 0
[ 344.007343] EC = 0x25: DABT (current EL), IL = 32 bits
[ 344.010380] Data abort info:
[ 344.013502] SET = 0, FnV = 0
[ 344.018788] ISV = 0, ISS = 0x00000004
[ 344.021650] EA = 0, S1PTW = 0
[ 344.024688] CM = 0, WnR = 0
[ 344.028501] Data abort info:
[ 344.031626] [000f02fa0202012a] address between user and kernel address ranges
[ 344.034574] ISV = 0, ISS = 0x00000004
[ 344.037441] Internal error: Oops: 96000004 [#1] PREEMPT SMP
[ 344.044538] CM = 0, WnR = 0
[ 344.048352] Modules linked in:
[ 344.053897] [000102080102020a] address between user and kernel address ranges
[ 344.056847] nf_conntrack_netlink nfnetlink vspm_if(O) vspm(O) mmngrbuf(O) mmngr(O)
[ 344.074629] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G W O 5.10.83-cip1-yocto-standard #1
[ 344.083722] Hardware name: Renesas SMARC EVK based on r9a07g044c2 (DT)
[ 344.090223] pstate: 00400005 (nzcv daif +PAN -UAO -TCO BTYPE=--)
[ 344.096213] pc : kfree+0x9c/0x370
[ 344.099518] lr : skb_free_head+0x2c/0x38
[ 344.103421] sp : ffff8000114eb9c0
[ 344.106719] x29: ffff8000114eb9c0 x28: ffff00000a8e4000
[ 344.112010] x27: ffff00001463c400 x26: 0000000000000000
[ 344.117301] x25: 0000000000000000 x24: ffff8000114ebbf8
[ 344.122592] x23: ffff800010a3e904 x22: ffff80001106bc38
[ 344.127883] x21: ffff00000c318000 x20: fb0f02fa02020102
[ 344.133174] x19: fffffe000010c600 x18: 0000000000000000
[ 344.138464] x17: 0000000000000000 x16: 0000000000000000
[ 344.143755] x15: 0000000000000001 x14: 00000000000000c0
[ 344.149045] x13: 0000000000000068 x12: 0000000000000000
[ 344.154335] x11: 0000000000000000 x10: 9a8b555e625f6764
[ 344.159626] x9 : 0000000000000001 x8 : 000000000000001b
[ 344.164916] x7 : 000000009706a8c0 x6 : 00000000000000e0
[ 344.170207] x5 : ffff00000fd07600 x4 : fffffdffbffc42a0
[ 344.175497] x3 : 0000000000009068 x2 : 0000000000000000
[ 344.180788] x1 : 0202fb6602fc0102 x0 : 0000000000000030
[ 344.186079] Call trace:
[ 344.188519] kfree+0x9c/0x370
[ 344.191473] skb_free_head+0x2c/0x38
[ 344.195033] skb_release_data+0x108/0x1a0
[ 344.199025] skb_release_all+0x28/0x38
[ 344.202758] kfree_skb+0x30/0x90
[ 344.205975] ip_rcv_finish_core.isra.26+0x198/0x390
[ 344.210830] ip_sublist_rcv+0xd0/0x1c8
[ 344.214562] ip_list_rcv+0x10c/0x1b0
[ 344.218124] __netif_receive_skb_list_core+0x194/0x228
[ 344.223240] netif_receive_skb_list_internal+0x188/0x2a0
[ 344.228528] gro_normal_list.part.207+0x20/0x40
[ 344.233038] napi_complete_done+0xc0/0x1e0
[ 344.237119] ravb_poll+0x154/0x420
[ 344.240504] net_rx_action+0x10c/0x360
[ 344.244237] efi_header_end+0x124/0x26c
[ 344.248057] irq_exit+0xc0/0xd0
[ 344.251187] __handle_domain_irq+0x68/0xc0
[ 344.255268] gic_handle_irq+0xc0/0x138
[ 344.258999] el1_irq+0xc8/0x180
[ 344.262128] arch_cpu_idle+0x18/0x28
[ 344.265688] default_idle_call+0x24/0x5c
[ 344.269595] do_idle+0x204/0x278
[ 344.272809] cpu_startup_entry+0x28/0x68
[ 344.276714] rest_init+0xd4/0xe4
[ 344.279930] arch_call_rest_init+0x10/0x1c
[ 344.284008] start_kernel+0x494/0x4c8
[ 344.287659] Code: 9ac022f7 b6b8091e aa1703d7 d503201f (b9402a80)
[ 344.293733] ---[ end trace ac5a7aeab11d114e ]---
[ 344.298330] Kernel panic - not syncing: Oops: Fatal exception in interrupt
[ 344.305175] SMP: stopping secondary CPUs
[ 345.392446] SMP: failed to stop secondary CPUs 0-1
[ 345.397214] Kernel Offset: disabled
[ 345.400686] CPU features: 0x0240026,2800a238
[ 345.404935] Memory Limit: none
[ 345.407978] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---

Along with this I have added wifi feature for that I am inserting kernel module. If my image doesn't have docker then all the functionality working fine but if I have docker feature added then kernel panic happens

Parents Reply Children
No Data