Dear Renesas Team,
I am using Hi-hope RZ/G2M evaluation board and I need to use USB 2.0 port as OTG.
I follow this link "renesas.info/.../RZG_DeviceTree" for kernel configuration. When I insmod usb_g_serial or any other gadget driver, I get error messages.
root@hihope-rzg2m:/# insmod /lib/modules/5.10.158-cip22-yocto-standard/kernel/drivers/usb/gadget/function/u_serial.ko
[ 439.899348] u_serial: Unknown symbol usb_ep_free_request (err -2)
[ 439.905590] u_serial: Unknown symbol usb_ep_alloc_request (err -2)
[ 439.911839] u_serial: Unknown symbol usb_ep_queue (err -2)
[ 439.917392] u_serial: Unknown symbol usb_ep_enable (err -2)
[ 439.923103] u_serial: Unknown symbol usb_ep_disable (err -2)
insmod: ERROR: could not insert module /lib/modules/5.10.158-cip22-yocto-standard/kernel/drivers/usb/gadget/function/u_serial.ko: Unknown symbol in module
root@hihope-rzg2m:/# insmod /lib/modules/5.10.158-cip22-yocto-standard/kernel/drivers/usb/gadget/legacy/g_serial.ko
[ 237.635631] g_serial: Unknown symbol usb_remove_function (err -2)
[ 237.641874] g_serial: Unknown symbol usb_get_function_instance (err -2)
[ 237.648547] g_serial: Unknown symbol usb_add_config_only (err -2)
[ 237.654695] g_serial: Unknown symbol usb_string_ids_tab (err -2)
[ 237.660740] g_serial: Unknown symbol usb_get_function (err -2)
[ 237.666593] g_serial: Unknown symbol usb_composite_unregister (err -2)
[ 237.673248] g_serial: Unknown symbol usb_put_function (err -2)
[ 237.679111] g_serial: Unknown symbol usb_add_function (err -2)
[ 237.684962] g_serial: Unknown symbol usb_composite_probe (err -2)
[ 237.691068] g_serial: Unknown symbol usb_composite_overwrite_options (err -2)
[ 237.698221] g_serial: Unknown symbol usb_otg_descriptor_alloc (err -2)
[ 237.704768] g_serial: Unknown symbol usb_put_function_instance (err -2)
[ 237.711398] g_serial: Unknown symbol usb_otg_descriptor_init (err -2)
[ 237.717858] g_serial: Unknown symbol usb_ep_autoconfig_reset (err -2)
insmod: ERROR: could not insert module /lib/modules/5.10.158-cip22-yocto-standard/kernel/drivers/usb/gadget/legacy/g_serial.ko: Unknown symbol in module
Note: No made in change in DTS file.
Looking forward to help to enable USB OTG port. Am I missing anything here?
Regards,
Dipen Patel