Hello Expert,
In yocto build of Renesas RZ/G2UL, it generates "tar.gz" image along with the bootloader and kernel images.
After that, we need to follow manual steps to partition the SD card and put the kernel and rootfs in seperate partition along with the DD of the bootloaders on initial sectors of SD card.
# sudo dd if=/dev/zero of=/dev/sda bs=1M status=progress # ./usb_sd_partition.sh # sudo dd if=bootparams-smarc-rzg2ul.bin of=/dev/sda seek=1 count=1 # sudo dd if=bl2-smarc-rzg2ul.bin of=/dev/sda seek=8 # sudo dd if=fip-smarc-rzg2ul.bin of=/dev/sda seek=128 # sudo cp Image-r9a07g043u11-smarc.dtb /media/embedded/RZ_FAT/ # sudo cp <Image>.bin /media/embedded/RZ_FAT/ # cd /media/embedded/RZ_ext/ # sudo tar jxvf <IMAGE>.tar.bz2
To avoid this manual process and do all the above processes in single common steps with command like "DD" (common way of other processor like NXP, TI ) way, do we have any WIC image generation WKS file?
How we can automate this process? (especially flash and prepare SD Card in Windows machine as well - with single wic or image file we can achieve that through different flash writer utility in Windows.)
A fast response would be appreciated.
Thanks and Regards,
Anil Patel
Hi Anil,WKS file to make WIC image is not supported yet in current BSP. But it will be supported soon.(It is also possible to make your own WKS file and add to current BSP).> How we can automate this…
Hi,
As the create_image.sh script in Chris's answer does,
egret said:U-boot can load the kernel and device tree from an ext4 partition.Also, I don't think SMARC RZ/G2UL board and the software support anything that requires a FAT partition (e.g. UEFI).Why…
Hi Anil,WKS file to make WIC image is not supported yet in current BSP. But it will be supported soon.(It is also possible to make your own WKS file and add to current BSP).> How we can automate this process?
Isn't a script file like your command list enough?
Hello HungT,Script file with listed command will not work on windows system.
For windows, wic image is suitable and expected behavior.
Is there any specific reason why we don't follow the standard yocto way for creating single file (like wic) and flash sd card and instead go with this manual process?
Thanks,
Anil
Hmmm, are you building the BSP with a Linux machine anyway?
This script will make an SD Card image file (like wic) that can be programmed by a Windows PC user.
https://github.com/renesas-rz/rzg2_bsp_scripts/tree/master/image_creator
In your case, it seems that you are writing bootparams, BR2, and FIP to an unused area (?) right after the master boot record, so I think it would be faster to change your script than to change the create_image.sh script.
BR
Thank you all for the response. I came to know that there is not wic file or wks rules for renesas yocto.
Can anyone please answer :
Anil said:When we expect to have support of WIC image?
WIC will be added from BSP v3.0.5
Anil said:Is U-Boot built correctly inside yocto? or it has to built outside of yocto (RZ/G2 Uboot and Trusted Firmware and creae srec and mot file) and flash? (Like a mention in my steps)
u-boot is built inside of Yocto, then packaged together with Trusted Firmware-A. The "FIP" image that you program contains u-boot.
Anil said:Is there any specific reason why we don't follow the standard Yocto way for creating single files (like wic) and flash sd card and instead go with this manual process?
This is my personal guess.
I think creating a WIC file is not very important for this device/board, so it is put on the back burner.
RZ/G2UL is designed to boot from eSD, eMMC, and quad SPI flash memory.The SMARC RZ/G2UL board includes all of these boot devices and we can try them out.However, I believe that, perhaps due to footprint, the eSD is replaced by an SD card holder that can also be used as external storage.
We can write the WIC file to the SD card using a utility on the host machine, but not to the blank eSD on the board. Also, in the case of a custom board equipped with RZ/G2UL, there may not be an eSD-compatible SD card holder.